Other Parts Discussed in Thread: TPA3140D2, LM4836
Hi,
I have TPA3140D2PWPEVM (Eval board for TPA3140D2) which I am using with a Bluetooth module. When I power up the Eval board, even if the Bluetooth module is turned off there is a continuous noise present.
This noise increase when I touch the J11 and J12 connectors.
Even after connecting Bluetooth with mobile, the noise remains. When playing audio, the audio level is much higher then the noise so noise is barely audible but when we pause audio, the noise is again heard.
I am using Bluetooth output and connecting it to male headers on eval board (L- and GND, R- and GND).
Load is 5W, 4ohm speaker, BTL mode.
LIMRATE is OFF, GAIN set is 32dB (I tried with different settings but could not see any change in audio levels), SS off 1 is selected.
Attached is waveform when there is no audio input (captured between L+ and GND)