Hi, I'm using LM4951A with a 4-ohm speaker as advised by TI support.
However, I note that at high volume setting, the amplifier is shutting down for hundreds of miliseconds.
This seems to be a current limiting rather than a thermal limiting factor as happens immediately.
I can't see in the datasheet if there is a current limit and to what value it's set to.
Perhaps the simple answer is that the part is not suitable for 4-ohm despite previous info.
Graph below shows the following signals.
Ch1: Vout- (pin6)
Ch2: Bypass (pin1)
Ch3: VDD (pin9)
it's noticeable that Vout- is turned off by the amplifier.