Other Parts Discussed in Thread: PCM4202EVM, PCM3070, PCM4202, OPA1632
I am looking to prototype a real-time wireless audio transmitter. I will want:
Tx:
24-bit 96kHz ADC (preferably 5V input signal range)
SPI/I2S/PCM/etc output
Onboard DSP/FPGA (optional)
Rx:
24-bit 96kHz DAC
Onboard DSP/FPGA (optional)
I already own some embedded dev boards which can handle wireless communication, but I'm looking to select the best solution for the audio codec side of things. Perusing the website, it looks like using an EVM is the best bet (PCM4202EVM, PCM3070EVM, etc), as it includes I/O jacks as well as powerful codecs, but I'm unsure which is the fastest while meeting all my minimum requirements. I would greatly appreciate guidance!
Regards,
Shandon