Hello
We are using TPA6203A1DGN to amplify the audio output of a GSM module. When we test the performance of TPA6203A1 using its evaluation module, everything is fine and audio quality is as required. Also, both OUT+ and OUT- pins have the same DC bias so that speaker is not DC loaded. However, when we try the same with a custom board, which has the same components as the evaluation module but only TPA6203A1DGN used in the fully differential mode, we observe that OUT- has a bias of VDD and OUT+ is at GND level. As expected, the speaker heats up because of the bias. As the datasheet implies the bias must have been handled by the common mode amplifier.
We would be really grateful if you could help us on this issue.
Best Regards
Yusein Ali