Dear TI Team.
I would like to hear the advice of TPA2080D1 because of POP noise during TEST.
Please refer to the following circuit.
Due to Fixed Gain, we have to reduce the input and add the resistor as above.
POP noise is generated by this.
Decreasing the resistance decreases the THD.
If the THD decreases, we will not be able to use it.
The cause of the pop noise is that the reference voltage rises at the same time when EN Pin goes high.
Is there a way to raise the reference voltage in advance?
please check.
Thanks.