This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5630 output power

Other Parts Discussed in Thread: TAS5630

Hi,

TAS5630 datasheet is specifying that PBTL output power is 600W at 2 ohm and 300W at 4 ohm. Based on this information I am calculating the voltage as P = V*V/R, V = Sq root (P*R), V = Sq root (600 * 2) = 35V rms. I am using this voltage to calculate the output power at 8 ohm (35*35/8 = 150W) and 16 ohm (35*35/16 = 75W). As per my calculations the power delivered to the 8 ohm load is 150W and 16 ohm load is 75W. Is this approach correct.

Regards,

Veera.