Other Parts Discussed in Thread: TAS6424-Q1
Hello
If use TAS6424-Q1 to drive four speaker, does AIC3254 could drive 4 speaker with TAS6424-Q1 by one I2S output? Thank you.
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
If use TAS6424-Q1 to drive four speaker, does AIC3254 could drive 4 speaker with TAS6424-Q1 by one I2S output? Thank you.
BR
Patrick
Hi, Patrick,
The 'AIC3254 is a Stereo audio codec, which is capable of sending up to two channels on the I²S bus, four channel digital output is not supported.
The only way to use a single 'AIC3254 to drive four channels on the '6424 would be to tie the digital output of the codec to the two digital inputs, that way the amplifier will drive four speakers, but will share the same stereo contend across channels 1/3 and 2/4.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer