This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3113D2: FAULT mode after power-up

Part Number: TPA3113D2


Hello,

 

I build the test board for the TPA3113D2 amplifier.

Unfortunately, power amp gong to the FAULT mode (when shorted to the SD pin no automatic recovery observed).

After power-up short PWM burst observed, after that no PWM, PINS 25 (18) VDC= 2V

Testing conditions:

VCC = 12V

Vin_disconnected.

Gain: 20db.

PLIMIT: 5V or shorted to GVDD.

GVDD=7V.

 

Thank you

Mark