Other Parts Discussed in Thread: TPA3116D2
Hello TI,
I'm using the TPA3116D2EVM with 12-18V PVCC and an 4-8ohm dummy load.
I've tried to replicate the measurements from the DS which are mostly with the BD Modulation (JP7 set) Mode.
When trying to measure the waveforms before and after the inductors without any load connected, I find the board constantly shutting down (JP3 is set).
Due to the DS this means three posibilities: (see attachment)
1. Over Current
2. Over temperature
3. High DC Offset
It can't be over current since my dc power supply is limited to 8A and I also don't think that it is the over temperature.
But I do find a DC Offset at the outputs (more on the right channel than on the left channel).
Then I have tried to use the 1SPW Modulation Mode which strangely works fine.
So my question is if I'm missing out something important to run the EVM in BD Modulation Mode.
If you need any more information please let me know.
Regards,
Jens