Other Parts Discussed in Thread: PCM1864-Q1
Hi Expert,
Why AIC3254Q1 can't meet -45~105 or 125 degree? But PCM1864Q1 can meet it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Why AIC3254Q1 can't meet -45~105 or 125 degree? But PCM1864Q1 can meet it.
Hi, Jerry,
The AIC3254-Q1 is an automotive device which has different features and considerations from the PCM1864-Q1. On the AEC-Q100 certification, there are different temperature grades given to the devices according to the supported operating temperature ranges.
The AIC3254-Q1 is a Temperature Grade 3 device which means the operating temperature goes from -40 to 85 degree, while the PCM1864-Q1 is certified as a Grade 1 device and can operate from -40 to 125 degrees.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer