This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TLV320AIC3XSW-LINUX: tlv320aic3x-codec 1-0018: Unable to sync registers 0x1-0x2. -11 dian, Rate 8000 Hz, Stereo aplay: pcm_write:2023: write error: Input/output error -- TLV320AIC3105

Part Number: TLV320AIC3XSW-LINUX
Other Parts Discussed in Thread: TLV320AIC3105

Tool/software: Linux

Dear TLV320AIC3XSW-LINUX Team

Could you please help me to get the responses for the threads that is  posted below?

Kindly do the needful as early as possible

Eagerly awaiting for your replies

Many Thanks in advance

  • Srini,

    Unfortunately the driver you are looking for help with was written for the TI Sitara processor which you are not using. The Sitara team can provide you with as much support with Sitara processors as you need including using the linux driver for the AIC3x with a Sitara processor. I can provide you with all of the TLV320AIC3105 configuration support or help with more detailed application questions. I am not able to provide support for the linux driver.

    The Sitara team provided you with a number of links that should help you resolve your issues. There are many linux communities online that might be able to help you.

    best regards,
    -Steve Wilson