Other Parts Discussed in Thread: TAS3251EVM, , TAS3251
Hi Andy,
I still have some questions about the memory of the miniDsp in TAS5756.
After reviewing the TAS3251EVM evaluation sheet I have to say that this AMPLI family is excellent and allows a lot of project flexibility with exceptional sound quality. One only drawback: if it had an internal memory it would be even simpler and more immediate!
Your suggestion would be to use the TI MSP430 micro-controller component. Is this component sufficient to maintain the memory of the pre-established configuration? Or do I also need to use an XMOS, that I see in the evaluation sheet?
Back to the TIMSP430 micro-controller: the functions as per Figure 5. TAS3251EVM Schematics (2 of 6) SW-MUTE SW-VOLUP -VOL DN ... and so on, are already set up in the micro-controller or do they need programming for each installed component?
Thank you so much for your feedback on the matter.
Eugenio