Other Parts Discussed in Thread: TAS3251, , MSP-EXP430FR2433
Hi,
I have a few questions regarding the TAS3251 and TAS3251EVM
I would like to use the TAS3251 with the TAS5756. They are connected both with I2S inputs and also I2C. Both work by turning them off and on; the memory is kept only on the TAS3251.
The I2C addresses are W98 x the 5756 and W94 for the 3251.
Using the TAS3251EVM evaluation card MPS430, can it manage two different TAS with different addresses?
What would you suggest as a solution? Does MPS430 have a pre-program option by default for basic commands like volume, input select, mute?
About the TIMSP430 micro-controller: the functions as per Figure 5. TAS3251EVM Schematics (2 of 6) SW-MUTE SW-VOLUP -VOL DN ... and so on, are already set up in the micro-controller or do they need programming for each installed component?
Thank you in advance,
Eugenio