Hi, I have done some evaluations with the PCM1865EVM board, with PPC2 in Windows. For now, I have some questions on the usage of this EVM board.
1. For now, PCM1865EVM provides three configurations, Mode 0/1/2, and I use it in Mode 2. But with PPC2, the configuration should be repeated in power-on/off/on circle. Can I flash the configuration to the board to make it works in Mode 2 once power-on this board?
2. PPC2 works in Windows OS, but I would like to do the evaluation in Linux OS. May I get one Linux version of PPC2?
3. As I would like to connect the PCM1865EVM board with my one another board, which is within Linux OS, may I do the configuration within instructions, without GUI operation? I mean if there is API documents to introduce the operation sequences on the PCM1865EVM board configuration.
Thanks.