This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3128D2: TPA3128D2: SE input typical schematic.

Part Number: TPA3128D2


PVCC is 12V,

Fault short to SD, and fault is 1.8V.

i worry is too high DC offset.

Can you help provide SE input typical schematic?

thanks!