This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4382: SRC4382 Bypass ASRC

Part Number: SRC4382

Hello

In order to keep the integrity of the digital inputs, could you please forward the signals coming from the DIR inputs and Port A I2S  directly to Port B without passing through the ASRC.

Example: Input DIR SP/DIF 48kHZ,Out PORTB I2S 48kHZ,Input DIR SP/DIF 96kHZ,Out PORTB I2S 96kHZ,.......

Input PORTA I2S 48kHZ,Out PORTB I2S 48kHZ,Input PORTA I2S 96kHZ,Out PORTB I2S 96kHZ,.......

  • welcome to e2e Forum!

    YES, SRC4382 can be configured for digital input at Port A can be routed to Port B. The audio serial ports are configured using control registers 0x03 through 0x06.

    In addition, we can also configure the output of DIR to be routed to Port B as described above.

    Best regards,
    Ravi