This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: What is the correct Clock Configuration

Part Number: TLV320ADC3101


Hi,

MCLK is 12.288MHz and i want that ADC_FS is set at 48kHz

So i disable PLL and CLOCK-GEN Muxing is set to MCLK.

%NADC: 1

%MADC:4

%AOSR:64

ADC_FS is then 48000Hz 

ADC_INTF_CTRL_2: is set to ADC_CLK(12.288MHz)

%N: 2

BCLK: 6.144MHz (I thought that 32bit x 2 Channels x 48000Hz x 2 )

Is BCLK correct? And how should i set the DOUT register?

 EDIT: I measured the PINS and BCLK is 6.144MHz, WCLK is 48kHz and DOUT is 48kHz

Shouldnt DOUT be 6.144MHz too?