This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA2311: PGA2311 power supply

Part Number: PGA2311
Other Parts Discussed in Thread: TPS7A49

Hello,

I'm designing a high end quality A class amp and would like to use PGA2311 to add digital volume control.

My design has separate analog ground for both channel in order to keep a very high channel seperation. Then I have few questions about the power sheme possibility of PGA2311.

First question: is it possible to have separate ground for PIN 10 and PIN 15? In fact I use small value resistor (0.1R) to isolate left and right channel ground this leading to a voltage drop around 0.15V for each channel when amp is ON (my general ground is connected to both 0.1R resistors to create channel left groung and channel right ground), this leading to a 0.3V voltage drop between PIN10 and PIN15, it's OK for PGA2311?

If i'ts OK to have separate voltage level between PIN10 and PIN15 how I connect bypass capacitors C3,C4,C5,C6 ?

Note: I use low noise LDOs (TPS7A49/30) to generate +/-5V analog rails for PGA2311, the ground reference level for these rails is my general ground.

Thanks for help!

Best regards,

Florian