Hello,
Just a short, simple question regarding these clocks. I will apply this codec as an interface between analog world and GSM module which outputs and inputs PCM signals. If I use this codec as a slave device and PCMCLK signal will be generated by a GSM module (128kHz or 2.048MHz) should I connect together MCLK and PCMCLK pins ? It is mentioned in a datasheet that in such a case they can be "tied together". But I just would like to be 100% sure about it.
Kind regards
Jacek