Hi Sir
My Application is re-sampling audio input(I2S) from Port A(32kHz~96kHz) to Port B(fixed in 48KHz) .
and set register like below
0x3 <= 8'b00000000
0x4 <= 8'b00000011
0x5 <= 8'b00011000
0x6 <= 8'b00000011
and MCK(pin 25) input is 12.288Mhz
48kHZ Audio(by i2S) pass to Port A interface , but no any output from Port B signal . and make sure the input(Port A) audio signal is correct .