This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6011A4: TPA6011A4 getting more power with same interface

Part Number: TPA6011A4
Other Parts Discussed in Thread: TAS5717

Should it be possible to have a high power (5-10W is enough) similar part with the same interface (headset output, speaker output, output selection based on headset connection, volumen control). I should accept a higher voltage power supply (12-24V). Kind regards,

  • Hi Juan,

    Welcome to e2e.
    There are some mid-power amps with speaker and headphone drivers, like TAS5717. Although the input for speaker driver is digital (I2S) and it is separate from headphone input and driver, which is all-analog.
    Perhaps another solution would be to use separate devices for speaker and headphone.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators