This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIX4192: interface between tlv320aic12k with dix 4192

Part Number: DIX4192


Hi,

Can I interface 8 number of tlv320 aic12k mono codec in cascade mode directly with DIX4192?

Requirement : transmit and receive 8 channels of voice over optical link

  • Hi Rojan,

    Welcome to e2e Forum!

    Can you please describe the system in a block diagram form as I do not seem to understand the full requirements for the same? 

    As far as DIX4192 goes, it has DIT which can take 2-ch audio input stream into an AES3-encoded output stream and DIR can handle four differential line recievers and uses 4:1 mux...it would be helpful to know more details in block diagram to answer your question.

    Thanks & Best regards,
    Ravi

  • Please find the attached simple block diagram of required system.