This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48312: Short to Battery and GND Protection

Expert 7280 points
Part Number: LM48312

Dear team,

Dear Ivan,

I have a similar case as below thread: using LM48312, I would need to be protected against short to VBAT (where VBAT is ~32V,  >> PVDD) and short to GND.

Can we suggest some external circuitry for this functionality ? (I am already aware of this app note  which won't cover this usecase since Vcc max is about 6V for LM48312)

Also, LM48312 datasheet mentions an "advanced output short circuit protection with auto-recovery", can someone share some details about this ?

Many thanks in advance!

Best regards,

PA