Other Parts Discussed in Thread: TAS5825M
Hi team,
Customer use TAS5754 and met some issue, please help give some comments.
1, If TAS5754's internal temperature sensor can read out data ?
2, When set EQ+DRC on TAS5754EVM by PPC2, it worked. Export this config and run target board, TAS5754 will not work good, audio can output, but no EQ+DRC. Question is, if PPC2 is right tools for export TAS5754M's config files?
3, Inside of TAS5754, if DRC function must work before volume control? It will be trouble when DRC is fixed but volumn need changed,because different volumn need modify DRC.
4, Use two 4OHM speaker(40W+40W) as load of TAS5754, audio output will be distortion, it is right?
5, When TAS5754 is working, if we pause the clock input, and then resume clock, device will keep work good again?
Thanks!