This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TLV320AIC3104: TLV320AIC3104IRHBR code question

Part Number: TLV320AIC3104


Tool/software: Code Composer Studio

Hi ti team,

    Could you pls help us check below question?thanks!

SCH as below

First,mic1 left input,Right_LOP/M putput

changed:

Used two channel,One mic1 left input to Right_LOP/M output,the Two mic1 right input to LEFT_LOP/M output

Currently, the input of intput1 cannot be turned off when the input2 channel is configured, and there are two mic inputs at the same time.

The configuration registers are as follows