This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6138A2: Thermal protection

Part Number: TPA6138A2


Hi expert,

 

I am checking with TPA6138A2 datasheet and not able to find a thermal protection function.

 

If the device runs a continuous full power output, like 3.3VDD, 16ohm, 10%THD, is there any concern regarding the reliability? It may get thermally damaged?

 

Thank you for your advice.

 

Best regards,

Daisuke KAWASAKI

  • Hi Kawasaki-san,

    The device operation should be within data sheet spec values, the Recommended Operation Conditions table gives a max ambient temp value of 85degC.
    At high temperatures, the output of the device is reduced (it is not disabled), so distortion due to clipping increases at higher temperatures.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators