Other Parts Discussed in Thread: TPA2006D1
Dear Team,
our customer is looking for a Class D speaker amp and the TPA2005D1 or TPA2006D1 seem to be a good candidate.
However, we try to understand the differences between the two versions.
- The 06 seems to have slightly better specs (Efficiency, PSRR, noise)
- The 06 seems to be a bit cheaper ($0.4 vs $0.35 @ 1k webprice)
- The 06 is compatible with 1.8V at the Shutdown pin
- The 05 has more package options
Do we see it correctly that the 06 is an improved version with less package options? Or do we miss a point?
Thanks and best regards
Martin