Hi!
My customer is developing a concept that mixes two I2S signals and outputs them as one I2S.
It is being tested using Purepath GDE and Purepath concole2.
Below is a block I made using GDE for testing.
However, I2S audio source mixed with ASI3 is not output (bit clock, word clock, D out)To do this, I used Purepath concole2 to change the ASI3 setting in Register Page4,
But I still have not found the properly solution.
For reference, change the block as shown below to change the I2S output to ASI1, and check that the digital out data is normally output.
But this is not what customers want.
The customer wants to change the mixed data to the required sampling frequency and output the I2S to ASI3.
Is there a solution that can solve this problem by changing other sets or modifying GDE blocks?
Thank you.
Best regards
From Anthony