This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3256EVM-U: The footprint of AIC3256_RHB_USB_EVM_REVA

Part Number: TLV320AIC3256EVM-U
Other Parts Discussed in Thread: TLV320AIC3256

Hi! I find the footprint of resistence and capacitance of  the TLV320AIC3256 codec moudle is 0603. I  want to replace them with the footprint of  0402. I want to know if it is feasible.

  • maolin shi,

    Are you asking if you can replace the capacitors on the EVM? If you bought the EVM, it is yours, you are welcome to change the capacitors if you feel as though you can do it.
    best regards,
    -Steve Wilson
  • Hello, Steve-Wilson!

    I mean I want to design my  own project based on the Schematics of the EVM (of course I has also bought the EVM). The footprints of  capacitors and resistance of the EVM is 0603 and they are a little bit big for my design. I will evaluate and try the footprint of 0402  for my design. Thank you for you help! 

    best regards,

    maolin.shi