Hello,
In my audio application the ADC portion and the optical inputs are working fine, but the coaxial inputs are not working. The voltage level from the DVD player seems to meet the 200mV minimum level, the input signal is terminated with a 75 ohm resistor and coupled to the PCM9211 through a 100nF capacitor as shown in a reference design. In one input I raised the level to about 500mV by changing the resistor to 300ohms it still wont work. The Coaxial power supply is turned on by writing 0x00 and 0x01 respectively to register 0x34. I think it worked once but after that it is not decoding the coaxial inputs.
Is there any other register I should set.
Regards,
John.
Mercy Electronic and Electrical Industries.
Bangalore, India.