I'm using TPA3118 to disign an amplifier, which is put near the speaker. Since output inductor can bring ilinar distortion, Can the output inductor and capacitor be removed? will this improve performance of speaker?(I know this may radiate 500khz radio to the air, but the more I care is sound quality.)
Besides, datasheet only shows performance in 400khz, but will the high-frequency performance be better if set freq at 1200khz? (e.x. will THD at 6khz low down?)
At last, may I ask why thd at 6khz is the highest, even higher than that of 15khz.
Thanks for your patient.