This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: output distortion

Part Number: TPA3255


Hi 

We are testing TPA3255 in 4 x SE mode with below condition

INPUT DC:50V & 12V

TPA3255 MODE:SINGLE END(M1&M2=HI)

Load=4ohm

the input signal is 1KHz tone.

The symptom 

when input voltage is 2.8Vpp ~ 4Vpp the output looks ok.

when input voltage is 4Vpp ~ 5Vpp we see distortion (please refer to the video attached below)

when input voltage > 6Vpp the output looks ok again. 

         This issue only happen to OUT_D while OUT_A, B and C are ok. Remove the 4 ohm load the issue disappear. 

The output waveform was capture at connector J102 Pin 4.

 Schematics and the video as the attachment below. Any idea what happen?

SCHEMATIC1 _ AMP1.pdf