Part Number: PCM1864-Q1
Other Parts Discussed in Thread: PCM1864, PCM1862
Dear expert,
I have 5 channel audio data (three microphone, and one stereo FM), due to the limited I2S/TDM port available on my application processor, I want to use PCM1864 + PCM1862 configured as TDM.
I see on PCM1864 datasheet page 73, one PCM1864 can be configured as clock master and another can be clock slave, like the picture below.
My question is, to save a crystal on PCM186x, can I use application processor as clock master without MCLK output, and let the two PCM186x to be clock slave, so that they both generate the required MCLK from BCLK?
Thank you.