Hello, I am considering doing a project on the wireless transmission of digital audio in the sub 1 GHz band. So the first step is to convert the analog audio into digital, and I see this codec TLV320ADC3101-Q1.
If I take samples at 44.1 kHz and the resolution of the conversion is 24 bits, I have a data rate of 1058.4 kbps, so my question is if the digital audio data is compressed and how much is it. Because I have to send it to the tranciver. I see some transceivers in IT, for example, the CC1350 that allows me to transfer 500 kbps of data in the band from 779 MHz to 930 MHz with 2-GFSK modulation, but I do not know if this transcriber is ideal for this project.
I see the MLX2571 that is used in professional wireless audio systems, but I can not find any information on the data rates, and I do not know if TI has development software for this product.
I ask here this information and guidance for this project, and if I have to have a more complex vision for him.
Thanks, and I'm waiting for an answer.