G'Day
We're designing an audio amp with multiple (4) TPA3255-Q1 devices. The (3) slaves will be sync'ed from the master.
We observe the (differential) oscillator/clock emitted from the master, Fosc is 6x the PWM frame rate, Fpwm. Each Fosc cycle therefore represents 1/6 of the PWM period or 60º. Fpwm would appear to be derived from Fosc via a divide by 6.
Referring to Table 7 in the datasheet (SLASEM8A) "Master/Slave Inter Channel Delay Settings" the Slave 1 delay is 60º, representing one Fosc period.
There does not appear to be a means (well, I can't find one) to sync the (internal) master PWM frame to the slaves, lest there be a 6:1 ambiguity of the slave PWM phase!
Q1. Are the slaves PWM frame somehow sync'ed to the master by some magic?
Q2. If the slaves PWM frames are not in sync with the master can a random multiple of 60º be expected after RESET?
Regards
David