This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2559EVM: Purepath 'Systemp checks" error

Part Number: TAS2559EVM
Other Parts Discussed in Thread: TAS2559

Hi

I run the TAS2559's "running hardware checks" The speaker test will fail as shown below.

I set the jumper to mono, and actually the sound is output to the device A speaker (the sound is a little small), but the GUI also becomes FAIL.

At first test, it seemed to be OK with CHECK. What problem is this?

Pleas check it.

Thank you.

Best regards.

From Anthony

  • Hi Anthony,

    Could you make sure that volume settings for EVM on your system is set to the maximum?
    Sometimes volume settings is not max and this could cause this issue.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators