This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5102EVM-U: Configuration without Windows

Part Number: PCM5102EVM-U
Other Parts Discussed in Thread: PCM5102

I'm trying to configure my PCM5102EVM to evaluate while using its optical or coaxial SPDIF inputs, but I don't own a Windows machine.  The manual for the EVM is pretty vague, so I'm looking for guidance to either configure it manually without connecting it to a computer, or to configure it through other means on my non-windows machine without running the CodecControl software.  The configuration changes I need to make are the most utterly basic, simply switching digital audio input sources, so I'm baffled as to why I'd need to use software that only runs on that one archaic operating system.  I'm a circuit designer, not a programmer, but I know there must be a way to to send commands to this thing from my modern computer.  Also, does the EVM store these configuration changes in the nonvolatile memory?

I'm thankful in advance for whatever help one of you is able to provide.