I have a opa134 soldered into a simple non-inverting opamp circuit shown below.
Input is 1Vp-p. The output is severely distorted unless the supply rails are increased to +/-15V. The datasheet says it can take +/-2.5V minimum. What am i missing?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a opa134 soldered into a simple non-inverting opamp circuit shown below.
Input is 1Vp-p. The output is severely distorted unless the supply rails are increased to +/-15V. The datasheet says it can take +/-2.5V minimum. What am i missing?
Hello Dylan,
You don't mention in the input voltage amplitude being applied to J1. You have the OPA134 set up as a non-inverting amplifier which exercises the input Common-Mode Voltage Range (Vcm) of the Op amp. For the OPA134 the linear input Common-Mode Voltage Range is specified from (V–)+2.5 to (V+)–2.5 V. Therefore, with +/-5 V supplies the Vcm range is approximately -2.5 V to +2.5 V. If those limits are exceeded the Op amp input stage is forced into non-linear operation and distortion will occur. You also need to make sure that the specified output voltage range isn't being exceeded as well.
Increasing the supply voltages increases the Vcm range and linear operation will be obtained provided the input signal's common-mode voltage stays within that range. Try reducing the input signal level and see if the distortion drops off.
Regards, Thomas
Precision Amplifiers Applications Engineering