Other Parts Discussed in Thread: , TMS320C5515
Hello,
I am looking to develop a digital stethoscope as per the TI implementation using the TLV320AIC3254 audio codec. I had some queries regarding this:
1. How do I operate power supply for this IC? As per my understanding 1V8 supply should work, but the maximum is 1v9. Is this correct?
2. The MDK uses I2C (for configuring) and I2S for data transfer. But it also has SPI enabled in it. Is there any difference in using the I2C & I2S interface as opposed to using SPI. Does it prevent me from using certain features?
3. The pull-up resistors used in the EVM are 2.7K pulled up to 3V3. In my custom board I am using 2 I2C buses, with 4.7K and 10K pullup respectively. Can I use the Codec IC on any of these buses without facing an issue?
4. What is the difference between evaluating using the TLV320AIC3254EVM-K and the Medical Development Kit containing this codec, specified on the digital steth application note?