This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4911Q-Q1: new device recommendation

Part Number: LM4911Q-Q1
Other Parts Discussed in Thread: TLV320AIC3254-Q1, OPA1641-Q1, OPA1612-Q1, OPA1662-Q1, OPA1642-Q1,

Dear team,

My customer wants to find a headphone amplifier, and the rating is Automotive. But there is only one device on ti.com. Do we have new devices about headphone amplifiers?

Thanks & Best Regards,

Sherry

  • Hi Sherry,

    There is no other Q1 headphone amplifier at this moment, let me check if we'll have something new.
    In addition, can customer use digital input instead of analog inputs? If they can use digital input perhaps TLV320AIC3254-Q1 can be an option as this device has headphone output.

    Another option would be to use op amps, some options are below:

    • OPA1641-Q1
    • OPA1612-Q1
    • OPA1662-Q1
    • OPA1642-Q1

    These op amps have rail-to-rail outputs, and they have different input architectures (Bipolar or JFET) and supply voltage ranges.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hi Ivan,

    The customer needs High Fidelity Stereo Headphone Amplifier, and they are not cost sensitive. Please check whether we have new devices. I will recommend the devices that you suggest to the customer. And I will also confirm with the customer if they can use catalog rating.

    Thanks & Best Regards,

    Sherry

  • Sherry,

    Unfortunately there are no new automotive graded headphone amplifiers coming out.

    Please let us know if customer finds the op amps suitable and/or confirm if they can use catalog devices so we can suggest some of them.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hi Ivan,

    Thanks for your reply!

    Ok, I will recommend the devices you recommended to the customer. Once I get the news, I will updates to you!

    Thanks & Best Regards,

    Sherry

  • Sherry,

    Please feel free to contact me with any updates or further customer questions to my email: ivan.salazar@ti.com

    I will mark this thread as solved since there are no more questions about LM4911Q-Q1.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators