This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV603: Differential input with Line out/Headphone out which can support more then 3Vrms output.

Part Number: DRV603
Other Parts Discussed in Thread: TPA6133A2, TPA6112A2

Hi Sir,

Could you please advise us a candidate which can compare with MAXIM MAX97220? 

Here are the requirements from our customer, they would like to find a part which can drive more than MAX97220, please refer to their request point:

1. Differential input

2. Support both Line out/  Headphone out

3. Output swing support more than 2.15Vrms

4. Output power support more than 125mW @32ohm, 1%THD+N.

BTW, I am not sure that DRV603 will be the best candidate or not... but it cannot support the impedance with the Headphone range right?

Looking forward to hearing from you soon.

Thanks,

George