I am having an issue with the frequency response of this amplifier. I tested the frequency response using a 70 mV rms single ended input signal from 256Hz to 200kHz, with a 24V rail voltage at 1.2MHz switching frequency. I have also made a couple measurements using the exact configuration as used in Figure 12 of the datasheet and still observed this spike in gain. Gain begins to increase as low as 35kHz and peaked at around 65kHz at 45db. I have not made any modifications to the TPA3116D2EVM board, so the gain is set for 26 dB. What is causing this pole in the frequency response?