Hi Team,
The typical application of DSD1792A is shown below with two 47uF decoupling caps on the VcomL and VcomR lines. How was the value of 47uF calculated and what would be the effect if the value of these caps was drastically decreased to 0.47uF? Is there a part number for a suggested cap to be used here?
Are these caps used for supply decoupling or are they functioning like the input capacitor for a buck converter (Class D amp)?
Also do the left and right channels operate independently? What degree of isolation is there between the two channels?
Regards,
Garret