Other Parts Discussed in Thread: LM1877
Hi Team,
We found there is output noise from LM4755 when connected to external pre-amp and larger speaker through RCA cable.
Usually LM4755 is connected to Speaker (~2W). My customer is designing a multifunction product, so it has to support RCA output (input resistor of RCA is 47k ohm)
Please imagine this use case is similar to "mobile phone supports internal speaker and also AUX OUT to external speaker"
Is there any suggestion to solve output noise issue?
Due to input voltage is 9V, only LM4755 and LM1877 can support this design requirement. In order to avoid output pop noise, it requires MUTE function. Therefore LM1877 can't meet. So my second question is : what if LM1877 is better solution than LM4755? will there be pop noise when connected to external speaker? Will there be output noise?