This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1692: The application of OPA1692D in MIC pre-amplifier circuit

Part Number: OPA1692


Hello sir,

May I ask whether OPA1692D is the good selection for MIC pre-amplifier circuit or not? If not, which one is recommended?

The production is platform microphone system with the features:

  • Power supply is 60W, built-in charging battery.
  • OPAMP is supplied by a single power supply from 12V to 15V.
  • Adding optional wireless block

Are there some applications notes/ reference design to talk about MIC pre-amplifier circuits or amplifiers' selections?