This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3122D2: info on protection parameters TPA3122D2

Part Number: TPA3122D2

hello, I'm using a TPA3122D2 BTL configuration for an amplifier with square wave input.
I'm feeding it at 17V and the load is composed of two 4 ohm speakers in series.
The problem that I am finding in some parts is that the current protection intervenes, because it feels that it detaches quickly and if the supply voltage is lowered a little, the protection no longer intervenes.
What I would like to ask is, what current value does the protection take, so that I can adjust before this phenomenon occurs.

Thanks
Andrew