Hello,
I've been working on reducing the power consumption for the AIC3111 audio codec. According to the datasheet, the registers [0][60] and [0][61] are responsible for the power consumption settings for the codec. I've created the header file using PPS, with a sample rate 8kHz. My default configuration is
// # reg[0][60] = 0x40 ; DAC programmable mode, DAC miniDSP powered up even if DAC is powered down
{ 60,0x40},
// # reg[0][61] = 0x00 ; ADC programmable mode
{ 61,0x00},
What is the 0x40 setting? There isn't any such mode on the datasheet.
Currently, my audio source is MIC1LP and I'm using SPL, and HPL,HPR as output. My current consumption is in the range of 25-35mA. I'd like to minimize this value and I couldn't really understand the datasheet on this subject. Is there any other reference I could check out or guidelines I could follow?