Other Parts Discussed in Thread: TLV3541
Hello,
I'm trying to extract SPDIF audio from the HDMI cable connected to the TV HDMI ARC port.
This will be the only function that I will be using with the PCM9211.
It seemed there was a technical note for the PCM9211 called SBAA300A.pdf, but I couldn't find it anywhere.
I'm assuming that the connection should be like below from the community's information.
My question is
1. Is this diagram correct?
2. Will this drawing be compatible with both HDMI 1.4 ARC and HDMI 2.1 eARC(No Dolby support and some limitation on data rate)?
3. Is there a recommended differential to single-ended converter?
Thanks in advance