Hello,
I plan using TLE2426 as a rail splitter in a OTA single supply application.
When I sim the schematic, there is no obvious problem.
However, I have 2 concerns :
1° What about the PSU bypass capacitors ?
Should they be placed from PSU to ground ONLY or from PSU to Virtual Ground AND from Virtual Ground to Ground ?
2° What about the current limitation of the TLE2426 ?
According to the sim, there is no issue, almost no DC current, if that is true, the only current to take into acount would be AC, which, in my application is ok (+/- 2mA)
Jean