Other Parts Discussed in Thread: TIPD177, PCM1690
Hello All,
I have been making a circuit based on the TI reference design TIPD 177 and I have a question regarding the circuit.
Attached is my schematics and it's mostly the same as the reference design.
I'm paralleling the differential current mode outputs from the DAC to improve the numbers and the summed output impedance of the output is around 50ohms. But the manufacturer said to be careful when connecting the paralleled outputs to the I/V stage opamps because it could be hard for op amps to keep the THD low. From my experiences and readings, it's best to have low output impedance from the DAC and high input impedance from the amp. Even the Voltage noise spectral density curve in the OPA1612 datasheet figure 32 shows lower noise when the source resistance is low.
The supply voltages are +/-12V and both are capable of supplying up to 1A currents.
Is this something that I just have to try out ?